FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation panel
FAQ
Operation panel
I input the start signal via the terminal STF and set the frequency using the setting dial. I set Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode) and Pr.79 (Operation mode) to "3".
When I press the "STOP" key on the operation panel, the motor is decelerated to stop and "PS" and "0.00" blink on the monitor. What happened?
When I press the "STOP" key on the operation panel, the motor is decelerated to stop and "PS" and "0.00" blink on the monitor. What happened?
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
This is because the protective function works to stop the motor. It is not a fault indication.
To cancel the protective function, turn OFF the start signal and press the "PU/EXT" button.
To cancel the protective function, turn OFF the start signal and press the "PU/EXT" button.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700