FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Output current value
FAQ
Output current value
Can I change the detection level of the output current value using a potentiometer or something similar?
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
The detection level of the output current value cannot be changed using a potentiometer or a similar device.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700