Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21790
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

What should I do not to operate the motor below a low speed (5 Hz)?
What happens if I set Pr.13 to "60 Hz", and the frequency to 30 Hz?
Category : 

Answer

Set Pr.13 (Starting frequency) or Pr.2 (Lower limit) to "5 Hz".

Also set Pr.10 (DC injection brake operation frequency) to "5 Hz".

The inverter does not operate if the starting frequency is 60 Hz and the setting frequency is 30 Hz.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries