Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21792
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I use the setting dial to set the frequency. The frequency changes when I turn the dial, but it returns to the previous value after flickering for several seconds.
I want to change the frequency just by turning the setting dial.
Category : 

Answer

Change Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode).  
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries