FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Programmable controller
FAQ
Programmable controller
I use Mitsubishi Q series programmable controller and connect three inverters to it.
What happens if the inverter is not powered ON?
What happens if the inverter is then powered ON?
What happens if the inverter is not powered ON?
What happens if the inverter is then powered ON?
- Category :
Answer
The error LED on the master side of the programmable controller blinks (faulty station present).
According to the SW80 station information, an error flag is attached to information of the station to which the powered OFF inverter is connected. (Check it with the mater side of the programmable controller.)
When the inverter is powered ON, communications automatically start and another network is established. Error LED turns off.
According to the SW80 station information, an error flag is attached to information of the station to which the powered OFF inverter is connected. (Check it with the mater side of the programmable controller.)
When the inverter is powered ON, communications automatically start and another network is established. Error LED turns off.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700