FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700P > Running frequency
FAQ
Running frequency
I operate the inverter by pressing the RUN key in the PU operation mode, but the running frequency does not increase over 120 Hz.
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
Check the setting of Pr.1 (Maximum frequency) and Pr.18 (High speed maximum frequency).
Pr.1 is initially set to "120 Hz".
Pr.1 is initially set to "120 Hz".
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700