Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21824
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

In CC-Link operation, is it possible to monitor the running frequency and output current simultaneously?  
Category : 

Answer

Yes. Set the first monitor code in the lower 8 bits and the second monitor code in the upper 8 bits of RWwn.
Set H6F to the first monitor code, and H70 to the second monitor code.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries