Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21825
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

In CC-Link operation, is it possible to set the running frequency continuously?
Category : 

Answer

Yes. However, write the setting data to the RAM of the inverter.
Set RWw1 in the setting value and turn ON the frequency setting command RYD.
To continuously set the frequency, keep the command RYD turned ON.
The setting completion RXD turns ON when writing completes. You can ignore it.
Note that if Pr.544 (CC-Link extended setting) is set to "0", when RYD and RYE turn ON simultaneously, RYD is prioritized.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries