Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21828
  • Release Date : 2018/08/22 16:29
  • Print

CC-Link

I consider performing CC-Link operation. Can the operation (start) commands be input both from PU and NET?
Category : 

Answer

The start commands cannot be input from both sources simultaneously because the operation command source is specified.
You can switch the command source as necessary.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries