Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21842
  • Release Date : 2018/08/22 16:29
  • Print

Frequency setting

I set the frequency to 40 Hz using the setting dial and operated the inverter.
After resetting the power, should I set the frequency again?
Category : 

Answer

When the frequency is set using the setting dial, it is not necessary to set it again.
The inverter memorizes the setting value internally even after the power reset.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries