FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Setting dial
FAQ
Setting dial
Can I use the setting dial of the inverter to set the frequency as well as change the parameter values?
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
Yes. You can use the setting dial of the inverter to set the frequency as well as change the parameter values.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700