FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > FR-E700
FAQ
FR-E700
I am considering to use the operation panel FR-PA02 for the FR-E500 by connecting it to the inverter with a cable. With the FR-E500, I used Pr.923 (Built-in frequency setting potentiometer gain) to calibrate the frequency setting of the built-in potentiometer. Which parameter should I use for the FR-E700?
- Category :
Answer
Use Pr.C24 (Frequency setting voltage gain frequency built-in potentiometer).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700