FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Frequency setting
FAQ
Frequency setting
I turn the setting dial to change the frequency, but it does not change.
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
When using the setting dial to set the frequency, turn the dial and display the frequency. Then, press the "SET" key while the desired value flickers.
The frequency is not set unless you press the "SET" key.
You can also set the potentiometer mode that does not require pressing the "SET" key but turning it to change the frequency. (Set Pr.161 to "1".)
The frequency is not set unless you press the "SET" key.
You can also set the potentiometer mode that does not require pressing the "SET" key but turning it to change the frequency. (Set Pr.161 to "1".)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700