FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Operation panel
FAQ
Operation panel
Can I attach the operation panel to the enclosure surface?
- Category :
Answer
The operation panels of the FR-E700, FR-D700, and FR-F700PJ are not detachable.
Therefore, it cannot be attached to the enclosure surface.
You can use the optional enclosure surface operation panel FR-PA07 and parameter unit PU07. Please consider these items. (The operation panel is detachable for the A700/F700 (P).)
Therefore, it cannot be attached to the enclosure surface.
You can use the optional enclosure surface operation panel FR-PA07 and parameter unit PU07. Please consider these items. (The operation panel is detachable for the A700/F700 (P).)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ