Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 21852
  • Release Date : 2018/08/22 16:29
  • Print

Operation mode setting

I want to input the operation signal by an external command and set the frequency using the setting dial and multi-speed setting.
How should I set the parameters?
Category : 

Answer

To enable the frequency setting with the setting dial and multi-speed setting, set Pr.79 to "3". Note that multi-speed setting is prioritized over setting using the setting dial. 
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?