FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > Operation mode setting
FAQ
Operation mode setting
I want to input the operation signal by an external command and set the frequency using the setting dial and multi-speed setting.
How should I set the parameters?
How should I set the parameters?
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
To enable the frequency setting with the setting dial and multi-speed setting, set Pr.79 to "3". Note that multi-speed setting is prioritized over setting using the setting dial.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700