Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21854
  • Release Date : 2018/08/22 16:29
  • Print

FR-DU07

Can I use the operation panel FR-DU07 that is supplied with the FR-F700 with the FR-E700, FR-D700, or FR-F700PJ?
Category : 

Answer

The FR-DU07 cannot be used with the FR-E700, FR-D700, or FR-F700PJ.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700, FR-D700, FR-F700PJ

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries