Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21857
  • Release Date : 2018/08/22 16:29
  • Print

FR-E700

I want to replace the FR-E500 with the FR-E700.
Is the operation panel of the FR-E700 is detachable like that of the FR-E500?
Category : 

Answer

The operation panel of the FR-E700 is not detachable because it is integrated.
The operation panel of the FR-E500 can be used with the FR-E700 by using the connection cable and back cover adapter set.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries