FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700PJ > PU operation
FAQ
PU operation
In PU operation, I want to use the setting dial like a potentiometer.
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
Set Pr.79 (Operation mode) to "1" (PU operation mode) and change Pr.161 (Frequency setting/key lock operation selection) to "1" (potentiometer mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700