FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-D700 > Terminal FM
FAQ
Terminal FM
Can I connect multiple meters (FS (full-scale 0 to 1 mA)) in series?
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
No. This is because the current cannot flow if the total internal impedance of the meter connected to the terminal FM is 300 Ω or higher.
You can connect multiple meters if the total internal impedance of the meter is less than 300 Ω.
You can connect multiple meters if the total internal impedance of the meter is less than 300 Ω.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700