FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A700 > CC-Link
FAQ
CC-Link
The Instruction Manual of the FR-A7NC instructs not to create an empty station number. Does this mean I should create reserved stations?
- Category :
Answer
It is OK if stations are set as reserved.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700