FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-F700 > Operation mode, PU operation mode switching
FAQ
Operation mode, PU operation mode switching
After changing the parameter setting value, I tried to switch to the PU operation mode and I failed.
I use the FR-A7NC.
I use the FR-A7NC.
- Category :
Answer
Change Pr.340 (Communication startup mode selection) from "1" to "0".
Power OFF and then ON the inverter.
Operate the inverter according to the value of Pr.79 (Operation mode).
Power OFF and then ON the inverter.
Operate the inverter according to the value of Pr.79 (Operation mode).
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-A700, FR-F700P, FR-F700