Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21904
  • Release Date : 2018/08/22 16:30
  • Print

CC-Link

I installed the CC-Link option FR-A7NC on the E700.
Can I change only the acceleration/deceleration time using the optional parameter unit FR-PU07?
Also, how can I use USB connection to allow for operating from the FR-Configurator?
Category : 

Answer

Set Pr.550 (NET mode operation command source selection) to "2" (PU connector is the command source).
When operating the inverter using the USB connector, set Pr.551 (PU mode operation command source selection) to "3" (USB connector is the command source).
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E700

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries