FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E700 > Frequency setting
FAQ
Frequency setting
I set up an external frequency setting potentiometer and the frequency with the potentiometer turned to the maximum position is initially set to 60 Hz. Can I change it to 90 Hz?
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
Set Pr.125 (Terminal 2 frequency setting gain frequency) = "90 Hz".
This changes the frequency with the potentiometer turned to the maximum position (at 5 V input) to 90 Hz.
This changes the frequency with the potentiometer turned to the maximum position (at 5 V input) to 90 Hz.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E700, FR-D700, FR-F700PJ, FR-A700, FR-F700P, FR-F700