FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Options > Using a higher grade power factor improving reactor
FAQ
Using a higher grade power factor improving reactor
Can I use the FR-BEL-1.5K instead of the FR-BEL-750)? Does the greater also serve for the lesser?
- Category :
Answer
Using a reactor under a load lighter than the rated capacity slightly spoils its effect in improving the power factor.
Therefore, you should use a reactor with the similar capacity to that of the motor.
Therefore, you should use a reactor with the similar capacity to that of the motor.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power factor improving reactor
- Series
- Option