FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-S500 > Speed 2 operation with potentiometer on operation panel
FAQ
Speed 2 operation with potentiometer on operation panel
Is speed 2 switching between the potentiometer on the operation panel and multi-speed operation possible?
During operation using the potentiometer, I want the inverter to decelerate before the operation edge and stop at the edge.
During operation using the potentiometer, I want the inverter to decelerate before the operation edge and stop at the edge.
- Category :
Answer
Yes. Set parameters as below.
For FR-E500
Set Pr.79 =3, and Pr.146= 0.
Multi-speed is prioritized.
For FR-S500
Set Pr.79 = 3, and Pr.53 = 1.
Multi-speed is prioritized.
For FR-E500
Set Pr.79 =3, and Pr.146= 0.
Multi-speed is prioritized.
For FR-S500
Set Pr.79 = 3, and Pr.53 = 1.
Multi-speed is prioritized.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-S500, FR-E500