Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 21998
  • Release Date : 2018/08/22 16:30
  • Print

Speed control failure due to 20 mA from DC 4

When I input 20 mA DC to the terminals 4 and 5, the speed only increases to around 47 Hz.
Pr.905 is set to 50 Hz (100%).
How should I adjust the setting?
Category : 

Answer

It seems that there is a read error for 20 mA DC inside the inverter.

Setting Pr.905 to 50 Hz while 20 mA DC is actually flowing between the terminals 4 and 5 allows for outputting 50 Hz.
Calibrate Pr.905 again.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-A100, FR-F500, FR-A200, FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries