FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-A500 > Coasting operation of the inverter
FAQ
Coasting operation of the inverter
With a system using the FR-A520 + FR-A5NC (CC-Link), I want to send the coasting command from the programmable controller. However, I cannot find the CC-Link assignment for this. How can I configure the system for this?
- Category :
Answer
To use an inverter using the external contact coast to stop (to shut off the inverter's output), short-circuit the terminals MRS and SD.
For CC-Link operation, this MRS signal (output stop function) is initially assigned to the device number RY9 (9th bit) and setting RY9 to "1" has the inverter to coast to stop.
For CC-Link operation, this MRS signal (output stop function) is initially assigned to the device number RY9 (9th bit) and setting RY9 to "1" has the inverter to coast to stop.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500