FAQ
FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FREQROL-E500 > Operation panel
FAQ
Operation panel
I want to remove the operation panel from the FR-E520-5.5K and attach it to a machine. What are the mounting dimensions?
Is the FR-E5P necessary for this purpose?
Can I use a commercial straight LAN cable for connection?
Is the FR-E5P necessary for this purpose?
Can I use a commercial straight LAN cable for connection?
- Category :
Answer
Be sure to use the FR-E5P to mount the operation panel.
This is because the board is bare on the back of the operation panel and a dedicated connector is required for cable connection.
You can use a commercial straight LAN cable for connection.
This is because the board is bare on the back of the operation panel and a dedicated connector is required for cable connection.
You can use a commercial straight LAN cable for connection.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500