Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22062
  • Release Date : 2018/08/22 16:30
  • Print

Vector inverter option

I want to use only the encoder output of the additional I/O function FR-VPA. Are pulses output when the motor rotates after just adding the option?
Category : 

Answer

Just by adding this option, encoder pulses connected to the inverter or option are output.
You can also divide the pulse train output.
Product Name
Inverter, magnet motor drive
Product Category
Plug-in option
Series
FR-V200

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries