Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22063
  • Release Date : 2018/08/22 16:30
  • Print

Err display on operation panel

Err display appears on the operation panel but the inverter continues operating normally.
It seems that the situation does not fall under any error cause described in the Instruction Manual. Are there any possible causes?
How can I clear this Err display?
Category : 

Answer

The following causes are probable for this Err display:
- Operation error (for example, you tried to input a value other than the available range of parameter values)
- RES signal is ON
- Communication fault due to connection fault between the inverter and operation panel

If the inverter can operate normally, the RES signal should be OFF. Check the operation procedure as well as check for a contact fault between the inverter and operation panel.
If both are correct, the operation panel or inverter may be faulty.
Contact your local distributor.
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries