Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22082
  • Release Date : 2018/08/22 16:30
  • Print

Inverter

I want to acquire transition data of frequency and current value while a motor is operating with a motor. Do you have any good ideal (or product)?
Since the inverter is installed in the operation section, I cannot visually check them.
Category : 

Answer

You can use the Hioki Memory HiCorder and clamp-on AC/DC high tester.
You can observe the inverter's frequency in one of the following two methods:
1. Attach the RC filter to the output from the terminals FM-SD.
2. Output from the terminals AM-5
(The terminal AM mentioned in 2. is only available with inverters equipped with the terminal AM, such as the FR-A500 series.)

Since you install the inverter in the operation section, the only recommended method is to install a Memory HiCorder in the operation section. (The inverter alone does not provide such a function.)
Product Name
Inverter, magnet motor drive
Product Category
Inverter
Series
FR-E500, FR-A500

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries