Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22090
  • Release Date : 2018/08/22 16:30
  • Print

Phase detection terminal

I cannot find the terminal block for the FR-RC-15K's phase detection terminal.
Where is the phase detection terminal (TB1-5)?
I found all other terminals.
Category : 

Answer

The phase detection terminal has been provided with units produced since December 1999.
You can identify these units with the serial number "N9Z○○○○○○" or later.
"N" is a symbol for the unit, "9" following it represents the year 1999, and "Z" represents December.

If your unit does not have the phase detection terminal, use the conventional wiring method.
Product Name
Inverter, magnet motor drive
Product Category
Power regeneration converter
Series
Option

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries