FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Extension of current sensor cable (EcoMonitorPlus/Light).
FAQ
Extension of current sensor cable (EcoMonitorPlus/Light).
Instruct a method for extending the cable between EcoMonitorPlus/EcoMonitorLight and split-type 5A current sensor (Model: EMU2-CT5, EMU2-CT5-4W).
Answer
Use an extension cable (Model: EMU2-CB-T1M / EMU2-CB-T5M/EMU2-CB-T10M / EMU2-CB-T1MS / EMU2-CB-T5MS / EMU2-CB-T10MS) for extending the cable between EcoMonitorPlus / EcoMonitorLight and split-type 5A current sensor.
It is extendable up to maximum 10m (Total interconnection length is 10.5m).
It is connected by phase wire system as follows:
It is extendable up to maximum 10m (Total interconnection length is 10.5m).
It is connected by phase wire system as follows:
1. In case of Single-phase 2-wire system / Single-phase 3-wire system / Three-phase 3-wire system.
2. In case of Three-phase 4 wire system.
* Two cables are included in the extension cable (separate type). It is possible to use two cables in combination.
Ex. Buy 5m of an extension cable (separate type) so as to make 10m cable by combining two cables.
Ex. Buy 5m of an extension cable (separate type) so as to make 10m cable by combining two cables.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
- As to ejecting an SD memory card.
- Method for creating a daily/monthly report using logging data (Model: EMU4-LM).
- As to Zero-Phase Current Transformer (ZCT) usable for the EcoMonitorPlus (Model: EMU4-LG1-MB).
- As to indication of the measurement value of the electric energy (EcoMonitorPlus/Light).