FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > As to logging period of the internal memory of the main unit.
FAQ
As to logging period of the internal memory of the main unit.
How long is the logging period of the internal memory of the main unit?
Answer
Logging period of the internal memory of the main unit as following:
1. In case of detailed data
Logging period differs according to logging cycle for detail data and the number of measuring circuits.
2. In case of 1hour data
Logging period differs according to the number of measuring circuits.
* It is the logging period where data is output at maximum volume.
1. In case of detailed data
Logging period differs according to logging cycle for detail data and the number of measuring circuits.
2. In case of 1hour data
Logging period differs according to the number of measuring circuits.
* It is the logging period where data is output at maximum volume.
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- Simultaneous data acquisition of MODBUS RTU communication and Optional Unit.
- As to compensation for power failure of Logging Unit for the Energy Measuring Unit.
- MEASURE LED not blink (EcoMonitorPlus).
- Method for measuring a circuit over 600A (EcoMonitorPlus/Light).
- As to changing location of the decimal point and units of the measured value.