FAQ
FAQAbout Products
- FAQ > Energy Saving Supporting Devices > Energy Saving Supporting Devices > Energy Measuring Units > Cause of "minus" indication for electric power value (EcoMonitorPlus/Light).
FAQ
Cause of "minus" indication for electric power value (EcoMonitorPlus/Light).
What causes assumed for "minus" display during electric power measuring ?
Answer
Following causes are assumed for the error.
1. Wrong orientation of the sensor?
2. 1-side and 3-side of the sensor are reversed?
3. Is connection between P1, P2 and P3, connection of P1 and P3 wrong?
4. Actually current flows in the regenerative direction?
1. Wrong orientation of the sensor?
2. 1-side and 3-side of the sensor are reversed?
3. Is connection between P1, P2 and P3, connection of P1 and P3 wrong?
4. Actually current flows in the regenerative direction?
- Product Name
- Energy Measuring Units
- Series
- EcoMonitor Plus, EcoMonitorLight
May I have your opinion?
Related FAQ
- As to simple measuring function of the EcoMonitorPlus (Model: EMU4-BM1-MB、EMU4-HM1-MB、EMU4-A2、EMU4-VA2).
- As to logging after removing an SD memory card.
- Setting of "Master / slave setting switch" (Model: EMU4-D65).
- As to timing for outputting data file into the SD memory card.
- As to periodic electric energy (EcoMonitorPlus/Light).