Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22259
  • Release Date : 2018/08/30 13:48
  • Print

Programmable controllers with no battery (MELSEC-F)

Which type of programmable controller from MELSEC-F series has no battery installed?
Category : 

Answer

A battery is used for backing up program memory and latched device data and maintaining clock operation in the event of a power failure.

The FX3S/FX3G/FX3GC series main units do not use a battery.
For the FX3G/FX3GC series main units, an optional battery can be used.
Product Name
FX1S, FX1N, FX1NC, FX2N, FX2NC, FX3S, FX3G, FX3GC, FX3U, FX3UC
Product Category
Main Unit, Accessories, Options
Series
MELSEC-F series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries