FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-F Series > I/O Extension > Input wiring (FX3 series)
FAQ
Input wiring (FX3 series)
Input terminals of the FX3 series are wired and the "X0" terminal and the "0V" terminal are short-circuited. However, the input does not turn on.
Answer
For the sink input, the "S/S" terminal and the "24V" terminal are needed to be short-circuited.
- Product Name
- FX3S, FX3G, FX3GC, FX3U, FX3UC
- Product Category
- Main unit, I/O Extension
- Series
- FX3S, FX3G, FX3GC, FX3U, FX3UC
May I have your opinion?
Related FAQ
- How to ground programmable controllers
- The power supply lamp of a running programmable controller suddenly turned off or flashes
- Multiple input COM terminals
- Using a specified bit (on/off) of a word device (D) as a condition for a contact
- Certificate of non-applicability to export MELSEC-F to other countries