Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22289
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the method to check the scan time

Answer

The current value of the scan time is stored in the following special devices. Please monitor using GX Works3.
◇Scan information
 SD520 Current scan time (ms)
 SD521 Current scan time (μs)
◇FX Compatible area
 SD8010 Current scan time(0.1ms)
Product Name
FX5U, FX5UC
Product Category
CPU Module, Engineering Software, GX Works3
Series
MELSEC iQ-F Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?