FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding UDP communication
FAQ
Regarding UDP communication
When communicating via UDP (such as socket communication) using the built-in Ethernet port, is broadcast communication supported?
Answer
The FX5 CPU module does not support UDP broadcast communication.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding Ethernet data-link
- Regarding the type of Ethernet connection cable
- Regarding expansion of communication ports
- Regarding the specifications of the built-in Ethernet function of FX5 CPU module
- Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3