Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22300
  • Release Date : 2018/08/30 13:55
  • Update : 2023/06/23 10:52
  • Print

Regarding the maximum number of controllable axes of the bulit-in positioning function

What is the maximum number of the axes that can be controlled with the built-in positioning function of FX5 CPU module?
Category : 

Answer

Up to 4 axes can be controlled. Please use a transistor output type CPU module.
(By adding a high speed pulse input/output module,
maximum 12 axes (CPU built-in 4 axes+expansion 2 axes×4 modules) can be configured.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Motion/Positioning
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries