FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Engineering Software > Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3
FAQ
Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3
Can the FX3 intelligent modules be selected on the module configuration diagram on GX Works3?
Answer
As the parameter settings of the FX3 intelligent function modules are not supported by GX Works3,
they cannot be selected from the element selection window.
Please use the configure using the program.
Also, regarding the setting and programming , please refer to the corresponding manual of each FX3 intelligent function modules.
they cannot be selected from the element selection window.
Please use the configure using the program.
Also, regarding the setting and programming , please refer to the corresponding manual of each FX3 intelligent function modules.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series