FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the maximum number of channels of high-speed counters
FAQ
Regarding the maximum number of channels of high-speed counters
Up to how many CHs can the FX5 CPU module's high-speed counter be controlled?
Answer
The FX5 CPU module's built-in high-speed counter can control up to 8CH.
Up to 16CH can be controlled by adding 4 modules of FX5-16ET/E□-H (high-speed pulse I/O module) to the FX5U/FX5UC/FX5UJ CPU module.
Up to 16CH can be controlled by adding 4 modules of FX5-16ET/E□-H (high-speed pulse I/O module) to the FX5U/FX5UC/FX5UJ CPU module.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding changing the current value of the high-speed counter.
- Regarding the settings of built-in analog function of FX5U CPU module
- Regarding the frequency of high-speed counters
- Regarding the digital output of the built-in analog function
- Regarding the number of available channels of the built-in high speeed counters.