Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22318
  • Release Date : 2018/08/30 13:55
  • Print

Regarding the system configuration FX5-CCL-MS with FX5 CPU module

Is it possible to connect two units of FX5-CCL-MS(CC-Link system master/intelligent device) to a single FX5U/FX5UC CPU module?
One as a master station and one as a intelligent device station.
Category : 

Answer

Yes, it is possible
Product Name
FX5-CCL-MS
Product Category
CPU Module, Network/Communication
Series
FX5U,FX5UC
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?