Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22323
  • Release Date : 2018/08/30 13:55
  • Update : 2023/06/26 09:04
  • Print

Regarding expansion of communication ports

Is is possible to add communication port to FX5 CPU module and use the MODBUS communication on multiple communication channels?
Category : 

Answer

It is possible to use the MODBUS serial communication with multiple channels.
However, only 1 channel can be set as the master.
The MODBUS serial communication settings can be set from GX Works3 parameters.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries