FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding expansion of communication ports
FAQ
Regarding expansion of communication ports
Is is possible to add communication port to FX5 CPU module and use the MODBUS communication on multiple communication channels?
Answer
It is possible to use the MODBUS serial communication with multiple channels.
However, only 1 channel can be set as the master.
The MODBUS serial communication settings can be set from GX Works3 parameters.
However, only 1 channel can be set as the master.
The MODBUS serial communication settings can be set from GX Works3 parameters.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series
May I have your opinion?
Related FAQ
- Regarding the specifications of the built-in Ethernet function of FX5 CPU module
- Regarding the function of a special relay.
- Regarding the system configuration of FX5-CCL-MS with FX5 CPU module
- Regarding the connection configuration of FX5-CCL-MS
- Regarding the maximum number of connections for MODBUS communication