Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22455
  • Release Date : 2018/09/03 17:28
  • Update : 2018/09/18 15:01
  • Print

Digit specification for bit devices in ST language with GX Works3

I want to create a program in ST language with GX Works3. How can I specify digits for a label of a bit device?
Category : 

Answer

For a label where digits are to be specified, set a bit type array as its data type. The following shows an example of when
a global label is used.
- Global label
 - Label name: Lamp
- Data type: Bit array of 16 elements
 - Device: Y100
- Program: Describe the digit specification of the bit device for a destination of the MOV instruction.

Product Name
MELSEC iQ-R Series
Series
MELSEC iQ-R Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries