FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
FAQ
Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
How long is the overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module?
- Category :
Answer
When the block number of the file register (R) is saved and stored, the overhead time becomes 35.9 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Models of batteries that can be used with MELSEC iQ-R series CPU modules
- Mounting Q series modules on a MELSEC iQ-R series base unit
- I/O numbers of a MELSEC iQ-R series I/O combined module (RH42C4NT2P)
- The number of times to insert and remove the extended SRAM cassette and SD memory card of a MELSEC iQ-R series CPU module
- Software to be supplied with GX Works3