FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Mounting Q series modules on a MELSEC iQ-R series base unit
FAQ
Mounting Q series modules on a MELSEC iQ-R series base unit
Can I mount Q series modules on a MELSEC iQ-R series base unit?
- Category :
Answer
You cannot mount Q series modules on a MELSEC iQ-R series base unit.
Use an RQ extension base unit (RQ65B, RQ68B, or RQ612B).
You cannot mount some modules, such as high speed data logger modules and network modules.
For details, refer to the following manual.
- MELSEC iQ-R Module Configuration Manual
1.1 Overall Configuration - System configuration specifications, configuration devices, and software
Use an RQ extension base unit (RQ65B, RQ68B, or RQ612B).
You cannot mount some modules, such as high speed data logger modules and network modules.
For details, refer to the following manual.
- MELSEC iQ-R Module Configuration Manual
1.1 Overall Configuration - System configuration specifications, configuration devices, and software
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Accessories of the MELSEC iQ-R series 40-pin connector type module
- Models of extended SRAM cassettes that can be used with MELSEC iQ-R series CPU modules
- Duplicated coil errors that can be checked with GX Works3
- Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
- Differences between GX Works3 and GX Works2