FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module
FAQ
Processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module
How long is the processing time of when multiple programs are executed with a MELSEC iQ-R series CPU module?
- Category :
Answer
When multiple programs are executed, the processing time (program switching time) becomes "Number of program files × 0.9 [us]".
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series
May I have your opinion?
Related FAQ
- Setting the MELSEC iQ-R series inter-module synchronization function
- Combination of the MELSEC iQ-R series inter-module synchronization function and the CC-Link IE Field Network synchronous communication function
- Parameters of GX Works3
- Including GX Developer in GX Works2
- Combination of the MELSEC iQ-R series inter-module synchronization function and the fixed scan communication of the multiple CPU system function